(bez PDV-a)
(s PDV-om)
Power supplies are a crucial aspect of any electrical equipment, providing reliable power to machinery, computers or other technology devices. A power supply changes a source electric current, such as a mains plug, to the correct voltage, frequency and current needed to operate the equipment safely.
A power supply is used to reduce mains or three phase electricity, often at 240 Vac or 440 Vac down to a voltage that is usable, such as 12 Vdc. The PSU also converts the current rating, in the form of AMPS, to a level that is safe for the device that is to be powered.
There are three main types of power supply: unregulated, linear and switch mode.
An unregulated power supply is the most basic type, they typically output a lot of ripple voltage (i.e. rapidly-varying instability) on the DC output power. If the input voltage varies, the output voltage will vary by a proportional amount. The advantage of an unregulated supply is that it's affordable, simple, and efficient.A linear power supply is similar in construction to an unregulated power supply, with the advantage of an added transistor circuit to regulate the output to a fixed voltage. A switch mode supply, also known as switching power supply, works by stabilising the mains electricity voltage in order to produce a clean, efficient and stable output voltage.
Power supply efficiency is known as the amount of power actually provided to the internal circuitry, divided by the amount of power drawn from the mains supply. If a PSU is 50% efficient and is required to provide 50 Watts of power, 100 Watts will be drawn from the main supply. The extra 50 W is lost as heat. A 90% efficient PSU would draw 56 W in the same circumstances.
Here are some common industries and environments power supplies can be used in:
(Kupujte 1344 proizvode)
(Kupujte 1344 proizvode)
(Kupujte 1581 proizvode)
(Kupujte 1581 proizvode)
(Kupujte 2 proizvode)
(Kupujte 2 proizvode)
(Kupujte 60 proizvode)
(Kupujte 60 proizvode)
(Kupujte 742 proizvode)
(Kupujte 742 proizvode)
(Kupujte 36 proizvode)
(Kupujte 36 proizvode)
(Kupujte 112 proizvode)
(Kupujte 112 proizvode)
(Kupujte 4398 proizvode)
(Kupujte 4398 proizvode)
(Kupujte 522 proizvode)
(Kupujte 522 proizvode)